Teamcenter Express Version 5.3 improves the productivity of manufacturing organizations for completing their design-through-manufacturing projects on-time and on-budget with support for the latest Teamcenter and Microsoft standards, many enhancements to the user interface, and expanded desktop integrations and project scheduling capabilities. These enhancements deliver improved productivity and profitability for managing everyday tasks for design-through-manufacturing from every user’s desktop and across multiple projects.
Teamcenter Express Version 5.3 is a configuration of the industry’s most widely implemented PLM solution, Teamcenter, delivering best-in-class scalability and performance to Teamcenter Express customers, and taking advantage of the latest developments in Teamcenter 8.3
“The release of Teamcenter Express 5.3 on the latest Teamcenter and Microsoft platforms adds significant capabilities to this comprehensive data management solution,” said Peter A. Bilello, President, CIMdata. “Extensive user interface enhancements should result in more efficient completion of common tasks and processes, and expanded integrations with desktop applications including Microsoft Office 2010 and Adobe Acrobat will enable more users to utilize their office automation tool of choice to work directly with a single source of managed product data, leading to improved collaboration and a reduction in errors in manufacturing.”
With support for the latest Microsoft and Teamcenter standards, Teamcenter Express users benefit from easy implementation based on their existing IT infrastructure, improved performance and low total cost of ownership.
The user interface has been updated to comply more closely with Windows standards for a faster learning curve and improved productivity. Some examples of the user interface improvements include:
The comprehensive Structure Manager module that is a standard part of Teamcenter Express has been enhanced so that a bill-of-material can be imported directly from Excel, creating new Items and a new product structure in Teamcenter Express. BOM capabilities have also been enhanced including markup of proposed changes and the ability to selectively apply or reject BOM markups
Teamcenter Express Version 5.3 supports wide access to a single source of product data from desktop applications through enhanced integrations with Microsoft Office and Adobe Acrobat, and a new utility to bulk load files.
Teamcenter Express V5.3 adds additional project scheduling capabilities that enable easier access for reviewing project status and enhanced project planning and cost analysis capabilities.
Decrease Text Size Enlarge Text Size Text Size
Teamcenter Express Version 5.3 fact sheet provides additional details of the new features and options in Teamcenter.
These demonstrations provide overviews of some of the key new capabilities of Teamcenter Express Version 5.3:
Press Release
Teamcenter Express Version 5.3
Av. Goiás, 1320 - São Caetano do Sul
Brasil, SP -
09521-300
(t): +55 (11) 4224-7155
Share this page through any of the following channels.