<?xml version="1.0" encoding="UTF-8"?>
<!-- 
Copyright 2008 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.
This software and related documentation are proprietary to 
Siemens Product Lifecycle Management Software Inc.
-->
<xsd:schema targetNamespace="http://www.plmxml.org/Schemas/PLMXMLSchema" xmlns:plm="http://www.plmxml.org/Schemas/PLMXMLSchema" xmlns:xsd="http://www.w3.org/2001/XMLSchema" elementFormDefault="qualified" attributeFormDefault="unqualified" xml:lang="en">
  <xsd:include schemaLocation="PLMXMLSchema.xsd"/>
  <xsd:annotation>
    <xsd:documentation>
    
                        PLMXML FD (FeatureDescriptions) Schema
                        
    Note: all length values are in metres, all angles are in radians.
    </xsd:documentation>
    <xsd:appinfo source="http://www.plmxml.org/Schemas/PLMXMLFDSchema">
      <plm:SchemaInfo name="PLMXMLFDSchema.xsd" date="2008-05-02" version="6.0" status="release"/>
    </xsd:appinfo>
  </xsd:annotation>
  <!-- -->
  <xsd:simpleType name="ThreadEntrySettingType">
    <xsd:annotation>
      <xsd:documentation>
      Thread Entry Setting.
      </xsd:documentation>
    </xsd:annotation>
    <xsd:restriction base="xsd:NMTOKEN">
      <xsd:enumeration value="standard"/>
      <xsd:enumeration value="straightPipe"/>
      <xsd:enumeration value="taperedPipe"/>
    </xsd:restriction>
  </xsd:simpleType>
  <!-- -->
  <xsd:simpleType name="ThreadExtentType">
    <xsd:annotation>
      <xsd:documentation>
      Thread Extent.
      
         finite:   of specific length
         toExtent: extent is that of the parent feature
      </xsd:documentation>
    </xsd:annotation>
    <xsd:restriction base="xsd:NMTOKEN">
      <xsd:enumeration value="finite"/>
      <xsd:enumeration value="toExtent"/>
    </xsd:restriction>
  </xsd:simpleType>
  <!-- -->
  <xsd:complexType name="ThreadType">
    <xsd:annotation>
      <xsd:documentation>
      This element describes a Thread.
      
      Note: the thread defaults to right-handed. An attribute to indicate left-handed
      may be added in the future if required.
      
      Attributes:
      
      type:              The type (standard) of thread. Some possible values are:
      
                            ANSI threads:      UNC, UNF, UNEF
                            ANSI pipe threads: NPSM, NPT
                            ISO threads:       M
                            ISO pipe threads:  Rp, Rc
                            
                         This attribute is a string to allow custom standards.
                             
      extent:            The extent type of the thread.
                             
      length:            The length of the thread, if extent = 'finite'.
      
      offset:            The offset distance, from the start of the owning feature,
                            before the thread starts.
                             
      nominalDiameter:   Nominal diameter, i.e. diameter of cylinder to which the
                            thread applies. 
      internalDiameter:  Diameter as applied to inside of thread.
      externalDiameter:  Diameter as applies to outside of thread. For these three 
                            diameters we have:
                            
                            internalDiameter .LT. nominalDiameter .LT. externalDiameter
      
      designateDiameter: Designated diameter. This is a string, e.g. "M8".
                            
      effectiveLength:   This is the length of the thread which is cut at full depth. 
      
      height:            The distance from the inside of the thread
                            to the outside of the thread. 
                         TODO: check if we need this as well is internal and externalDiameter?
                            
      taperAngle:        The angle of taper, in radians. This is positive
                            and less than pi/2. The taper is always towards the
                            centreline, in the direction of the thread.

      pitch:             The distance between adjacent threads, measured
                            along the length of the thread, in metres (SI units).
      </xsd:documentation>
    </xsd:annotation>
    <xsd:complexContent>
      <xsd:extension base="plm:AttribOwnerBase">
        <xsd:attribute name="type" type="xsd:string" use="optional"/>
        <xsd:attribute name="extent" type="plm:ThreadExtentType" use="optional"/>
        <xsd:attribute name="length" type="xsd:double" use="optional"/>
        <xsd:attribute name="offset" type="xsd:double" use="optional"/>
        <xsd:attribute name="nominalDiameter" type="xsd:double" use="optional"/>
        <xsd:attribute name="internalDiameter" type="xsd:double" use="optional"/>
        <xsd:attribute name="externalDiameter" type="xsd:double" use="optional"/>
        <xsd:attribute name="designateDiameter" type="xsd:string" use="optional"/>
        <xsd:attribute name="effectiveLength" type="xsd:double" use="optional"/>
        <xsd:attribute name="height" type="xsd:double" use="optional"/>
        <xsd:attribute name="taperAngle" type="xsd:double" use="optional"/>
        <xsd:attribute name="pitch" type="xsd:double" use="optional"/>
      </xsd:extension>
    </xsd:complexContent>
  </xsd:complexType>
  <!--  -->
  <xsd:complexType name="CounterSinkType">
    <xsd:annotation>
      <xsd:documentation>
      This element specifies a CounterSink component of a HoleFeature. The CounterSink
      starts with a given diameter and tapers down.
      
      Attributes:
      
      diameter:     The diameter of the start of countersink.
      
      angle:        The angle of the countersink. This is the angle between a line
                       lying in the cone of the CounterSink, and a plane through the
                       start of the CounterSink. The range is 0 to pi/2. For example, 
                       just below pi/2 would be a nearly-cylindrical CounterSink.
                       
      length:       The length of the countersink along its axis.
                       
      Elements:
      
      EntityRef:    Reference to entities that are related to the CounterSink
      </xsd:documentation>
    </xsd:annotation>
    <xsd:complexContent>
      <xsd:extension base="plm:AttribOwnerBase">
        <xsd:sequence>
          <xsd:element ref="plm:EntityRef" minOccurs="0" maxOccurs="unbounded"/>
        </xsd:sequence>
        <xsd:attribute name="diameter" type="xsd:double" use="optional"/>
        <xsd:attribute name="angle" type="xsd:double" use="optional"/>
        <xsd:attribute name="length" type="xsd:double" use="optional"/>
      </xsd:extension>
    </xsd:complexContent>
  </xsd:complexType>
  <!-- -->
  <xsd:complexType name="CounterBoreType">
    <xsd:annotation>
      <xsd:documentation>
      This element specifies a CounterBore component of a HoleFeature. 

      Attributes:
       
      diameter:        The diameter of the CounterBore.
      length:          The length of the CounterBore.

      Elements:
       
      EntityRef:       Reference to entities that are related to the CounterBore
      Thread:          Definition of thread for CounterBore (at most one)
      </xsd:documentation>
    </xsd:annotation>
    <xsd:complexContent>
      <xsd:extension base="plm:AttribOwnerBase">
        <xsd:sequence>
          <xsd:element ref="plm:EntityRef" minOccurs="0" maxOccurs="unbounded"/>
          <xsd:element name="Thread" type="plm:ThreadType" minOccurs="0"/>
        </xsd:sequence>
        <xsd:attribute name="diameter" type="xsd:double" use="optional"/>
        <xsd:attribute name="length" type="xsd:double" use="optional"/>
      </xsd:extension>
    </xsd:complexContent>
  </xsd:complexType>
  <!-- -->
  <xsd:simpleType name="HoleExtentType">
    <xsd:annotation>
      <xsd:documentation>
      Extent of hole, i.e. how its length is determined.
      
        throughAll:     through all faces
        throughNext:    through to the next face in the model
        fromTo:         between specified points
        finite:         from a specified point for a specified length
      </xsd:documentation>
    </xsd:annotation>
    <xsd:restriction base="xsd:NMTOKEN">
      <xsd:enumeration value="throughAll"/>
      <xsd:enumeration value="throughNext"/>
      <xsd:enumeration value="fromTo"/>
      <xsd:enumeration value="finite"/>
    </xsd:restriction>
  </xsd:simpleType>
  <!-- -->
  <xsd:complexType name="HoleComponentType">
    <xsd:annotation>
      <xsd:documentation>
      A component of a HoleFeature.
      
      Attributes:
       
      diameter:       The diameter of the hole.
      length:         The length of the hole.
      extent:         The way the hole length was determined. 
                         
      blindHoleAngle: The angle of the termination of the a blind hole. This is the
                         total angle at the tip, in radians, so pi would be a flat tip.
                         If omitted, the termination is flat.
      taperAngle:     The angle of taper, in radians. This is positive
                         and less than pi/2.

      Elements:
      
      Thread:         Definition of Thread(s) for hole component
    </xsd:documentation>
    </xsd:annotation>
    <xsd:complexContent>
      <xsd:extension base="plm:AttribOwnerBase">
        <xsd:sequence>
          <xsd:element ref="plm:EntityRef" minOccurs="0" maxOccurs="unbounded"/>
          <xsd:element name="Thread" type="plm:ThreadType" minOccurs="0" maxOccurs="unbounded"/>
        </xsd:sequence>
        <xsd:attribute name="diameter" type="xsd:double" use="optional"/>
        <xsd:attribute name="length" type="xsd:double" use="optional"/>
        <xsd:attribute name="extent" type="plm:HoleExtentType" use="optional"/>
        <xsd:attribute name="taperAngle" type="xsd:double" use="optional"/>
        <xsd:attribute name="blindHoleAngle" type="xsd:double" use="optional"/>
      </xsd:extension>
    </xsd:complexContent>
  </xsd:complexType>
  <!-- -->
  <xsd:complexType name="HolePositionType">
    <xsd:annotation>
      <xsd:documentation>
      This specifies the position, and optionally the direction, of a Hole.
      
      Attributes:
      
      position:       Position of the start of the hole in global 3-space coords.
      direction:      Direction of of the hole. This direction defines the reference
                         direction when evaluating the sequence of HoleComponent, 
                         CounterSink and CounterBore elements; and the extent/offsets 
                         values within those items. If absent, the direction attribute 
                         on the HoleFeature is used.
    </xsd:documentation>
    </xsd:annotation>
    <xsd:complexContent>
      <xsd:extension base="plm:IdBase">
        <xsd:attribute name="position" type="plm:VectorType" use="required"/>
        <xsd:attribute name="direction" type="plm:VectorType" use="optional"/>
      </xsd:extension>
    </xsd:complexContent>
  </xsd:complexType>
  <!-- -->
  <xsd:simpleType name="HoleOrientationType">
    <xsd:annotation>
      <xsd:documentation>
      The way in which the orientation of a hole is determined.
       
         normalToEntrySurface:      normal to the face in which the hole lies
         normalToPlacementPlane:    normal to a defined plane (not specified)
         coaxial:                   coaxial with another hole (not specified)
      </xsd:documentation>
    </xsd:annotation>
    <xsd:restriction base="xsd:NMTOKEN">
      <xsd:enumeration value="normalToPlacementPlane"/>
      <xsd:enumeration value="normalToEntrySurface"/>
      <xsd:enumeration value="coaxial"/>
    </xsd:restriction>
  </xsd:simpleType>
  <!-- -->
  <xsd:complexType name="HoleFeatureType">
    <xsd:annotation>
      <xsd:documentation>
      This is a Hole Feature. It may consist of a number of actual holes, each of which
      has the same sequence of Components (HoleComponent, CounterSink, CounterBore), but
      which may have differing positions and directions.
      
      Attributes:
      
      direction:      Direction of of the hole. This direction defines the reference
                         direction when evaluating the sequence of hole, countersink and
                         counterbore elements; and the extent/offsets values within those
                         elements. Individual HolePosition elements may override this 
                         direction. 

      sequenceRefs:   The sequence of HoleComponent, CounterSink and CounterBore elements 
                         that make up the complete hole description, in order along the
                         Hole axis. These elements must be sub-elements of this HoleFeature.
                        
      orientation:    The orientation of the hole with respect to the starting geometry. 
                         This is for information/presentation purposes. 
                        
      Elements:
      
      HolePosition:   One HolePosition element per actual hole. At least one.
       
      HoleComponent:  Definition of a HoleComponent
      CounterBore:    Definition of a CounterBore component
      CounterSink:    Definition of a CounterSink component
      </xsd:documentation>
    </xsd:annotation>
    <xsd:complexContent>
      <xsd:extension base="plm:FeatureBase">
        <xsd:sequence>
          <xsd:element name="HolePosition" type="plm:HolePositionType" maxOccurs="unbounded"/>
          <xsd:choice maxOccurs="unbounded">
            <xsd:element name="HoleComponent" type="plm:HoleComponentType"/>
            <xsd:element name="CounterBore" type="plm:CounterBoreType"/>
            <xsd:element name="CounterSink" type="plm:CounterSinkType"/>
          </xsd:choice>
        </xsd:sequence>
        <xsd:attribute name="direction" type="plm:VectorType" use="optional"/>
        <xsd:attribute name="sequenceRefs" type="xsd:IDREFS" use="required"/>
        <xsd:attribute name="orientation" type="plm:HoleOrientationType" use="optional"/>
      </xsd:extension>
    </xsd:complexContent>
  </xsd:complexType>
  <xsd:element name="HoleFeature" type="plm:HoleFeatureType" substitutionGroup="plm:Feature"/>
  <!-- -->
  <xsd:complexType name="ThreadedFeatureType">
    <xsd:annotation>
      <xsd:documentation>
      This is a Thread Feature, not associated with a Hole. Only a single position
      and direction can be specified.
      
      Attributes:
      
      position:       Position of the start of the thread in global 3-space coords
      direction:      Direction of the thread. This direction defines the reference
                         direction when evaluating the sequence of thread elements; 
                         and the extent/offsets values within those items.
      sequenceRefs:   The sequence of thread elements that make up the complete 
                         thread description. These elements must be defined as elements 
                         within this thread description.
      inside:         'true' if a thread feature on the inside of a hole, 'false' if
                         a thread feature on a boss.
      setting         The thread entry setting.
                       
      Elements:
      
      Thread:         Definition of a thread component. More than one is allowed.
      </xsd:documentation>
    </xsd:annotation>
    <xsd:complexContent>
      <xsd:extension base="plm:FeatureBase">
        <xsd:choice maxOccurs="unbounded">
          <xsd:element name="Thread" type="plm:ThreadType"/>
        </xsd:choice>
        <xsd:attribute name="position" type="plm:VectorType" use="required"/>
        <xsd:attribute name="direction" type="plm:VectorType" use="optional"/>
        <xsd:attribute name="sequenceRefs" type="xsd:IDREFS" use="required"/>
        <xsd:attribute name="inside" type="xsd:boolean" use="optional"/>
        <xsd:attribute name="setting" type="plm:ThreadEntrySettingType" default="standard"/>
      </xsd:extension>
    </xsd:complexContent>
  </xsd:complexType>
  <xsd:element name="ThreadedFeature" type="plm:ThreadedFeatureType" substitutionGroup="plm:Feature"/>
  <!-- -->
  <xsd:complexType name="FeatureDescriptionsType">
    <xsd:annotation>
      <xsd:documentation>
      This is a collection (sequence) of Features.
      
      Attributes:
      
      firstFeature:    The first feature in the sequence.
      ownerRef:        Reference to owning ProductRevisionView or Representation.
 
      Elements:
      
      Feature:         A HoleFeature or any other elements derived from Feature.
      </xsd:documentation>
    </xsd:annotation>
    <xsd:complexContent>
      <xsd:extension base="plm:AttribOwnerBase">
        <xsd:choice minOccurs="0" maxOccurs="unbounded">
          <xsd:element ref="plm:Feature" minOccurs="0" maxOccurs="unbounded"/>
        </xsd:choice>
        <xsd:attribute name="firstFeature" type="xsd:IDREF" use="optional">
			<xsd:annotation>
				<xsd:appinfo source="http://www.plmxml.org/tools/CodeGenerator">validate=skipName</xsd:appinfo>
			</xsd:annotation>
        </xsd:attribute>
        <xsd:attribute name="ownerRef" type="plm:anyURIType" use="optional"/>
      </xsd:extension>
    </xsd:complexContent>
  </xsd:complexType>
  <xsd:element name="FeatureDescriptions" type="plm:FeatureDescriptionsType" substitutionGroup="plm:AttribOwner"/>
</xsd:schema>