<?xml version="1.0" encoding="UTF-8"?>
<!-- 
  Copyright 2006 UGS Corp. All Rights Reserved.
  This software and related documentation are proprietary to UGS Corp.
-->
<xsd:schema xmlns:xsd="http://www.w3.org/2001/XMLSchema" xmlns:plm="http://www.plmxml.org/Schemas/PLMXMLSchema" targetNamespace="http://www.plmxml.org/Schemas/PLMXMLSchema" elementFormDefault="qualified" attributeFormDefault="unqualified" xml:lang="en">
      <xsd:include schemaLocation="PLMXMLSchema.xsd"/>
      <xsd:annotation>
        <xsd:documentation>
          PLM XML Motion Schema

          Motion results are defined in terms of sequences of frames. PLM XML
          imposes no connection between or order on the sequences of frames but
          an external application may do so via ApplicationRef elements.
        </xsd:documentation>
        <xsd:appinfo source="http://www.plmxml.org/Schemas/PLMXMLSchema">
          <plm:SchemaInfo name="PLMXMLMotionSchema.xsd" date="2006-04-28" version="6.0" status="release"/>
        </xsd:appinfo>
      </xsd:annotation>
      <!-- -->
      <!-- ******************** FrameSequence ****************************** -->
      <!-- -->
      <xsd:complexType name="FrameSequenceType">
        <xsd:annotation>
          <xsd:documentation>
            A sequence of Frames that defines Motion results definition.
            FrameSequences are independent.
            
            Attributes:
            
            frameRate:      The frame rate in frames per second (SI units).
            timeStamp:      The time in seconds (SI units) of the first Frame in
                            the sequence with respect to some external datum.
              
            Sub-elements:
            
            Frame:          The Frames in the sequence.
          </xsd:documentation>
        </xsd:annotation>
        <xsd:complexContent>
          <xsd:extension base="plm:AttribOwnerBase">
            <xsd:choice minOccurs="0" maxOccurs="unbounded">
              <xsd:element ref="plm:Frame"/>
            </xsd:choice>
            <xsd:attribute name="frameRate" type="xsd:double" use="optional"/>
            <xsd:attribute name="timeStamp" type="xsd:double" use="optional"/>
          </xsd:extension>
        </xsd:complexContent>
      </xsd:complexType>
      <xsd:element name="FrameSequence" type="plm:FrameSequenceType" substitutionGroup="plm:AttribOwner"/>
      <!-- -->
      <!-- ******************** FrameTypeEnum ****************************** -->
      <!-- -->
      <xsd:simpleType name="FrameTypeEnum">
        <xsd:annotation>
          <xsd:documentation>
            The type of a Frame, either simple (the default) or key.
          </xsd:documentation>
        </xsd:annotation>
        <xsd:restriction base="xsd:NMTOKEN">
          <xsd:enumeration value="simple"/>
          <xsd:enumeration value="key"/>
        </xsd:restriction>
      </xsd:simpleType>
      <!-- -->
      <!-- ******************** Frame ************************************** -->
      <!-- -->
      <xsd:complexType name="FrameType">
        <xsd:annotation>
          <xsd:documentation>
            A Frame of type simple represents a single Frame at the time of the
            previous frame plus the reciprocal of the frame rate in seconds (SI
            units). A Frame of type key represents a key Frame that is linearly
            interpolated at the frame rate up to the time of the previous frame
            plus the duration in seconds (SI units).
            
            Attributes:
            
            type:           The type of a Frame, either simple (the default) or
                            key.
            duration:       The time in seconds (SI units) of a Frame relative
                            to the previous frame.
            
            Sub-elements:
            
            MotionEntityRef: The references to the MotionEntity elements, which
                            represent the conceptual motion entities or bodies.
          </xsd:documentation>
        </xsd:annotation>
        <xsd:complexContent>
          <xsd:extension base="plm:AttribOwnerBase">
            <xsd:choice minOccurs="0" maxOccurs="unbounded">
              <xsd:element ref="plm:MotionEntityRef"/>
            </xsd:choice>
            <xsd:attribute name="type" type="plm:FrameTypeEnum" default="simple"/>
            <xsd:attribute name="duration" type="xsd:double" use="optional"/>
          </xsd:extension>
        </xsd:complexContent>
      </xsd:complexType>
      <xsd:element name="Frame" type="plm:FrameType" substitutionGroup="plm:AttribOwner"/>
      <!-- -->
      <!-- ******************** MotionTransformEnum ************************ -->
      <!-- -->
      <xsd:simpleType name="MotionTransformEnum">
        <xsd:annotation>
          <xsd:documentation>
            Specifies whether the Transform sub-element of a MotionEntityRef is
            applied to one or more conceptual motion entities or bodies
            absolutely or relatively (the default).
          </xsd:documentation>
        </xsd:annotation>
        <xsd:restriction base="xsd:NMTOKEN">
          <xsd:enumeration value="absolute"/>
          <xsd:enumeration value="relative"/>
        </xsd:restriction>
      </xsd:simpleType>
      <!-- -->
      <!-- ******************** MotionEntityRefType ************************ -->
      <!-- -->
      <xsd:complexType name="MotionEntityRefType">
        <xsd:annotation>
          <xsd:documentation>
            Applies a Transform sub-element to one or more conceptual motion
            entities or bodies. A MotionEntityRef may have an absolute or
            relative Transform.

            Attributes:

            transformType:  Specifies whether the Transform sub-element is
                            applied to the MotionEntity elements referenced by
                            the motionEntityRefs attribute absolutely or
                            relatively (the default). An absolute
                            MotionEntityRef applies its Transform to the
                            MotionEntity elements in the absolute coordinate
                            system. A relative MotionEntityRef applies its
                            Transform relative to the positions and orientations
                            of the MotionEntity elements in a previous Frame.
                            Those positions and orientations are usually defined
                            by the Transform sub-element of a MotionEntityRef in
                            a previous Frame. However, if no previous Frame has
                            a MotionEntityRef that applies to the MotionEntity
                            elements and that has a Transform sub-element, the
                            positions and orientations are defined by the
                            playback application.
            motionEntityRefs: References MotionEntity elements, which represent
                            the conceptual motion entities or bodies.

            Sub-elements:

            Transform:      The Transform that is applied to the MotionEntity
                            elements referenced by the motionEntityRefs
                            attribute.
          </xsd:documentation>
        </xsd:annotation>
        <xsd:complexContent>
          <xsd:extension base="plm:AttribOwnerBase">
            <xsd:choice minOccurs="0" maxOccurs="1">
              <xsd:element ref="plm:Transform"/>
            </xsd:choice>
            <xsd:attribute name="transformType" type="plm:MotionTransformEnum" default="relative"/>
            <xsd:attribute name="motionEntityRefs" type="plm:uriReferenceListType" use="optional"/>
          </xsd:extension>
        </xsd:complexContent>
      </xsd:complexType>
      <xsd:element name="MotionEntityRef" type="plm:MotionEntityRefType" substitutionGroup="plm:AttribOwner"/>
      <!-- -->
      <!-- ******************** MotionEntity ******************************* -->
      <!-- -->
      <xsd:complexType name="MotionEntityType">
        <xsd:annotation>
          <xsd:documentation>
            A conceptual motion entity or body.
            
            Attribute:
            
            entityRef:      References Occurrences in the Product Structure or
                            external references.
            
            Sub-elements:
            
            Reference:      Any references to entities within Occurrences.
          </xsd:documentation>
        </xsd:annotation>
        <xsd:complexContent>
          <xsd:extension base="plm:AttribOwnerBase">
            <xsd:choice minOccurs="0" maxOccurs="unbounded">
              <xsd:element name="Reference" type="plm:GDEReferenceType"/>
            </xsd:choice>
            <xsd:attribute name="entityRefs" type="plm:uriReferenceListType" use="optional"/>
          </xsd:extension>
        </xsd:complexContent>
      </xsd:complexType>
      <xsd:element name="MotionEntity" type="plm:MotionEntityType" substitutionGroup="plm:AttribOwner"/>
    </xsd:schema>