<?xml version="1.0" encoding="UTF-8"?>
<!-- 
Copyright 2008 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.
This software and related documentation are proprietary to 
Siemens Product Lifecycle Management Software Inc.
-->
<xsd:schema targetNamespace="http://www.plmxml.org/Schemas/PLMXMLSchema" xmlns:plm="http://www.plmxml.org/Schemas/PLMXMLSchema" xmlns:xsd="http://www.w3.org/2001/XMLSchema" elementFormDefault="qualified" attributeFormDefault="unqualified" xml:lang="en">
  <xsd:include schemaLocation="PLMXMLSchema.xsd"/>
  <xsd:annotation>
    <xsd:documentation>
    
                        PLM XML Delta Schema
                        
    </xsd:documentation>
    <xsd:appinfo source="http://www.plmxml.org/Schemas/PLMXMLDeltaSchema">
      <plm:SchemaInfo name="PLMXMLDeltaSchema.xsd" date="2008-05-02" version="6.0" status="release"/>
    </xsd:appinfo>
  </xsd:annotation>
  <!-- -->
  <!-- DeltaOperation -->
  <!-- -->
  <xsd:complexType name="DeltaOperationBase" mixed="true" abstract="true">
    <xsd:annotation>
      <xsd:documentation>
      Base class for elements which define Delta operations, 
      i.e. DeltaAdd, DeltaDelete, DeltaModify, DeltaReplace
      </xsd:documentation>
      <xsd:appinfo source="http://www.plmxml.org/tools/CodeGenerator">allowMixed=true</xsd:appinfo>
    </xsd:annotation>
  </xsd:complexType>
  <!-- -->
  <!-- Add -->
  <!-- -->
  <xsd:complexType name="DeltaAddType" mixed="true">
    <xsd:annotation>
      <xsd:documentation>
      This element represents adding a fragment of PLMXML, i.e. a tree of elements, to
      a master document.
      
      The sub-elements of this element are all added.
      
      Attributes:
      
      parentRef:       A URI reference to a placeholder element which represents the
                       element in the master document which will become the parent of the
                       added elements. Exactly one of parentRef or siblingRef should be present.
                       
      siblingRef:      A URI reference to a placeholder element which represents the
                       element in the master document which will become a sibling
                       of the added elements. There is no implication that the added element
                       will be adjacent to the sibling element in the sub-element ordering -
                       only that it will have the same parent.
      
      Elements:
      
      Any PLMXML elements may be included as sub-elements.
      </xsd:documentation>
      <xsd:appinfo source="http://www.plmxml.org/tools/CodeGenerator">allowMixed=true</xsd:appinfo>
    </xsd:annotation>
    <xsd:complexContent>
      <xsd:extension base="plm:DeltaOperationBase">
        <xsd:sequence>
          <xsd:any namespace="##any" maxOccurs="unbounded" processContents="skip"/>
        </xsd:sequence>
        <xsd:attribute name="parentRef" type="plm:anyURIType" use="optional"/>
        <xsd:attribute name="siblingRef" type="plm:anyURIType" use="optional"/>
      </xsd:extension>
    </xsd:complexContent>
  </xsd:complexType>
  <!-- -->
  <!-- Replace -->
  <!-- -->
  <xsd:complexType name="DeltaReplaceType" mixed="true">
    <xsd:annotation>
      <xsd:documentation>
      This element represents replacing a fragment of PLMXML, i.e. a tree of elements, with
      another tree.
      
      The sub-element of this element is used to replace the target element and all its
      descendents.
      
      Attributes:
      
      targetRef:       A URI reference to a placeholder element which represents the
                       element in the master document which will be replaced.
      
      Elements:
      
      Any PLMXML element may be included as sub-element. There must be exactly one.
      </xsd:documentation>
      <xsd:appinfo source="http://www.plmxml.org/tools/CodeGenerator">allowMixed=true</xsd:appinfo>
    </xsd:annotation>
    <xsd:complexContent>
      <xsd:extension base="plm:DeltaOperationBase">
        <xsd:sequence>
          <xsd:any namespace="##any" maxOccurs="unbounded" processContents="skip"/>
        </xsd:sequence>
        <xsd:attribute name="targetRef" type="plm:anyURIType" use="required"/>
      </xsd:extension>
    </xsd:complexContent>
  </xsd:complexType>
  <!-- -->
  <!-- Delete -->
  <!-- -->
  <xsd:complexType name="DeltaDeleteType" mixed="true">
    <xsd:annotation>
      <xsd:documentation>
      This element represents deleting a fragment of PLMXML, i.e. a tree of elements, from
      a master document.
      
      NOTE that it also removes any IDREF or local URI references to those elements, since 
      normally you would not want 'dangling' references left. For example, deleting an Instance 
      will automatically remove that Instance from any 'instanceRefs' attributes which reference
      it. 
      
      Attributes:
      
      targetRefs:       A multiple URI reference to placeholder element(s) which represent the
                        elements in the master document which will be deleted, along with
                        their sub-elements.
      </xsd:documentation>
      <xsd:appinfo source="http://www.plmxml.org/tools/CodeGenerator">allowMixed=true</xsd:appinfo>
    </xsd:annotation>
    <xsd:complexContent>
      <xsd:extension base="plm:DeltaOperationBase">
        <xsd:attribute name="targetRefs" type="plm:uriReferenceListType" use="required"/>
      </xsd:extension>
    </xsd:complexContent>
  </xsd:complexType>
  <!-- -->
  <xsd:simpleType name="DeltaModifyOpType">
    <xsd:restriction base="xsd:NMTOKEN">
      <xsd:enumeration value="replace"/>
      <xsd:enumeration value="add"/>
      <xsd:enumeration value="remove"/>
      <xsd:enumeration value="delete"/>
      <xsd:enumeration value="modifyUserData"/>
      <xsd:enumeration value="setOwner"/>
    </xsd:restriction>
  </xsd:simpleType>
  <!-- -->
  <!-- Modify -->
  <!-- -->
  <xsd:complexType name="DeltaModifyType" mixed="true">
    <xsd:annotation>
      <xsd:documentation>
      This element represents modifying an element in a master document in some way, 
      depending on the 'op' attribute.
            
      Attributes:
      
      targetRef:        A URI reference to a placeholder element which represents the
                        element in the master document which will be modified.
                        
      attributeName:    The name of the attribute being modified, if any.
      
      values:           The value or values to be used when modifying the attribute. The way in 
                          which this is used to make the modification is determined by the 
                          'op' attribute. 
                          
      valueRefs:        URI reference to placeholder element(s) which represent
                          elements in the master document; or to elements in Add or Replace
                          blocks in this delta. The attribute being modified is
                          altered to reference these elements, according to the value of the
                          'op' attribute.
                          
      op:               This determines the operation used to make the modification. One of
      
                        'replace'        completely replaces an existing attribute value, with 
                                         the value in 'values' or 'valueRefs'.
                        'add'            adds the values in 'values' or 'valueRefs' to an existing
                                         attribute, for example an integer array, IDREFS or multiple
                                         URI attribute.
                        'remove'         removes the values in 'values' or 'valueRefs' from an
                                         existing attribute.
                        'delete'         deletes an existing attribute entirely.
                        
                        'modifyUserData' merges the UserData of this Modify element into the 
                                         UserData of the target element. 'attributeName' is
                                         not set in this case.
      </xsd:documentation>
      <xsd:appinfo source="http://www.plmxml.org/tools/CodeGenerator">allowMixed=content</xsd:appinfo>
    </xsd:annotation>
    <xsd:complexContent>
      <xsd:extension base="plm:DeltaOperationBase">
        <xsd:sequence>
          <xsd:any namespace="##any" maxOccurs="unbounded" processContents="skip"/>
        </xsd:sequence>
        <xsd:attribute name="targetRef" type="plm:anyURIType" use="optional"/>
        <xsd:attribute name="op" type="plm:DeltaModifyOpType" default="replace" use="optional"/>
        <xsd:attribute name="attributeName" type="xsd:string" use="optional"/>
        <xsd:attribute name="values" type="xsd:string" use="optional"/>
        <xsd:attribute name="valueRefs" type="plm:uriReferenceListType" use="optional"/>
      </xsd:extension>
    </xsd:complexContent>
  </xsd:complexType>
  <!-- -->
  <!-- ExternalReference -->
  <!-- -->
  <xsd:complexType name="ExternalReferenceType">
    <xsd:annotation>
      <xsd:documentation>
      This element is a reference to an object in an Application data model. At present it 
      identifies the object by containing one or more ApplicationRef or NGID sub-elements.
      
      Attributes:
      
      type:           Optional PLMXML type of the external object, e.g. "ProductRevision"
      
      select:         If this attribute is present, it will be an XPATH string, which 
                      identifies the referenced object relative to a parent object, which 
                      is identified by the ApplcationRef sub-elements. The XPATH string will
                      be in terms of the PLMXML schema, but it will be interpreted as 
                      applying to the Application data model.
      SubElements:
      
      NGID:           Contains an identifier in NGID format.
      </xsd:documentation>
    </xsd:annotation>
    <xsd:complexContent>
      <xsd:extension base="plm:AttribOwnerBase">
        <xsd:sequence>
	      <xsd:element name="NGID" type="xsd:string" minOccurs="0"/>
        </xsd:sequence>
        <xsd:attribute name="type" type="xsd:string" use="optional"/>
        <xsd:attribute name="select" type="xsd:string" use="optional"/>
      </xsd:extension>
    </xsd:complexContent>
  </xsd:complexType>
  <xsd:element name="ExternalReference" type="plm:ExternalReferenceType" substitutionGroup="plm:AttribOwner"/>
  <!-- -->
  <!-- DeltaOperationGroup -->
  <!-- -->
  <xsd:complexType name="DeltaOperationGroupType">
    <xsd:annotation>
      <xsd:documentation>
      NB This is an extension to the DELTA schema included here to avoid
      the need for a separate schema.
      
      A group of Delta Operations. A context can be provided by adding an
      ApplicationRef sub-element of this element.
      
      SubElements:
      
      Add:            Add elements, representing the addition of a tree of elements
      Replace:        Replace elements, representing the replacement of a tree of elements
      Delete:         Delete elements, representing the deletion of trees of elements
      Modify:         Modify elements, representing an alteration to an attribute of
                        an element.
      </xsd:documentation>
    </xsd:annotation>
    <xsd:complexContent>
      <xsd:extension base="plm:DescriptionBase">
        <xsd:choice minOccurs="0" maxOccurs="unbounded">
          <xsd:element name="Add" type="plm:DeltaAddType"/>
          <xsd:element name="Replace" type="plm:DeltaReplaceType"/>
          <xsd:element name="Delete" type="plm:DeltaDeleteType"/>
          <xsd:element name="Modify" type="plm:DeltaModifyType"/>
        </xsd:choice>
      </xsd:extension>
    </xsd:complexContent>
  </xsd:complexType>
  <xsd:element name="DeltaOperationGroup" type="plm:DeltaOperationGroupType"/>
  <!-- -->
  <!-- PLMXMLDelta -->
  <!-- -->
  <xsd:complexType name="PLMXMLDeltaType">
    <xsd:annotation>
      <xsd:documentation>
      The top-level element in a PLMXML Delta file. This represents a delta, or change,
      to be applied to a PLMXML file or equivalent Application model (the 'master' file/model).
      
      Attributes:
      
      context:        A URI or other indication of the master Document or model to which 
                      this delta is to be applied.
      
      SubElements:
      
      Add:            Add elements, representing the addition of a tree of elements
      Replace:        Replace elements, representing the replacement of a tree of elements
      Delete:         Delete elements, representing the deletion of trees of elements
      Modify:         Modify elements, representing an alteration to an attribute of
                        an element.
                        
      ExternalReference:    References to Application objects. 
      </xsd:documentation>
    </xsd:annotation>
    <xsd:complexContent>
      <xsd:extension base="plm:DocumentBase">
        <xsd:choice minOccurs="0" maxOccurs="unbounded">
          <xsd:element name="Add" type="plm:DeltaAddType"/>
          <xsd:element name="Replace" type="plm:DeltaReplaceType"/>
          <xsd:element name="Delete" type="plm:DeltaDeleteType"/>
          <xsd:element name="Modify" type="plm:DeltaModifyType"/>
          <xsd:element ref="plm:ExternalReference"/>
          <xsd:element ref="plm:DeltaOperationGroup"/>
        </xsd:choice>
        <xsd:attribute name="context" type="xsd:string" use="optional"/>
      </xsd:extension>
    </xsd:complexContent>
  </xsd:complexType>
  <xsd:element name="PLMXMLDelta" type="plm:PLMXMLDeltaType"/>
  <!-- -->
</xsd:schema>