Zollner is one of the world’s top 15 Electronic Manufacturing Services (EMS) providers. Since 2002, Zollner’s process planners have used systems for material flow simulation. These systems were later complemented with tools for 3D visualized ergonomics studies and layout plans. However, growing customer requirements and Zollner’s desire for a stronger focus on full system manufacturing called for implementing an integrated solution capable of handling increasingly more information. To meet its requirements, Zollner established a benchmark project in which the production processes of an existing product were validated within a live test that lasted several months. Siemens’ Tecnomatix® software was the test system that proved its worth.
Red Bull Racing’s development process has to be as swift and precise as their vehicles, and the company relies on NX™ software for CAD/CAM/CAE and Teamcenter® software to capture and manage knowledge. It is a creative and collaborative, virtual world from which the real, live car emerges almost fully formed and ready to be put to the test on the track. “We call it our digital backbone,” says Steve Nevey. “NX and Teamcenter sit at the heart of the company and they feed data to our manufacturing facilities; we could not manage without them.”
Jaakonkatu 2
01620 Vantaa
Finland
(v): +358-9-540 4840
Share this page through any of the following channels.