Find out more about the powerful new functionality in Femap v11 in one of our demonstrations.

Some aspects of finite element modeling in Femap are shown in the following demos including composites, contact, complex loading, and meshing.

The following demos show some of the powerful preprocessing functionality in Femap including linking CAD data with Solid Edge.

Femap’s extensive analysis support, such as design optimization and metal forming can be viewed in the following demos.

The following demos show some of the powerful postprocessing functionality in Femap including beams and the Postprocessing Toolbox.

These demos give you an introduction to the use of the Entity Selector functionality in Femap. Also included is an overview of the Model Information tree in the Femap user interface as well as Tool Bars and Windows Tabbing and Pinning.

See how you can customize Femap to add functionality or transfer data to or from external programs like Excel with the API (application programming interface) and macro capability.
Decrease Text Size Enlarge Text Size Text Size
Tips and tricks that will help you work with Femap more effectively and boost your productivity.
(tel): +55 11 4228-7643
Share this page through any of the following channels.