Jack's Task Analysis Toolkit is a set of ten ergonomics analysis tools that help you design industrial tasks for optimal safety and productivity. An add-on to Jack® 2.2i, the Task Analysis Toolkit provides tools for:
The Low Back Spinal Force Analysis tool helps you evaluate the spinal forces acting on a virtual human's lower back, under any posture and loading condition. Based on a complex biomechanical low back model incorporating the latest anatomical and physiological data, the tool enables you to:
The Static Strength Prediction tool helps you evaluate the percentage of a worker population that has the strength to perform a task based on posture, exertion requirements and anthropometry. Based on strength studies performed over 25 years at the University of Michigan Center for Ergonomics, the Strength Prediction tool:
The NIOSH Lifting Analysis tool helps you evaluate symmetrical and asymmetrical lifting tasks, including lifts with less than optimal couplings between the object and the worker's hands. Based on NIOSH lifting equations developed by a committee of experts, the tool:
The Predetermined Time Analysis tool helps you predict the time required to perform a job by subdividing a task into a set of motions which have been assigned times based on the methods-time measurement (MTM-1) system. With this tool you can:
The Rapid Upper Limb Assessment (RULA) tool helps you evaluate the exposure of workers to the risk of upper limb disorders. For a given manual task, RULA:
The Metabolic Energy Expenditure tool helps you predict the metabolic energy expenditure requirements of a job based on worker characteristics and a description of the simple tasks that comprise the job. Based on the research of Garg, Chaffin and Herrin, this tool enables you to:
The Manual Handling Limits tool helps you evaluate and design manual handling tasks involving lifting, lowering, pushing, pulling and carrying for reduced risk of low back pain. Based on 20 years of research conducted at the Liberty Mutual Research Center, the tool enables you to:
The Fatigue and Recovery Analysis tool helps you assess whether enough recovery time is available for a given job to avoid worker fatigue. Based on strength and fatigue studies undertaken by Rohmert, the tool computes the recovery time required for a job and compares it to available rest time. If there is not enough rest time in a job cycle to accommodate recovery time, workers are assumed to be at risk of fatigue. With the Fatigue and Recovery Analysis tool, you can:
The OWAS tool provides you with a simple method for quickly checking the comfort of working postures and determining the urgency of taking corrective measures. Based on the Ovako Working Posture Analysis System (OWAS), the tool:
(tel): +55 11 4224-7196
Share this page through any of the following channels.