Concurrent engineering shaved two and a half years off development of the PC-21 training aircraft
Founded on December 16, 1939 in a meeting room of the Nidwaldner Kantonalbank, Pilatus Aircraft Ltd began as a small supplier to the Swiss Air Force. Since then, the niche supplier has become a global leader for the supply of singleengine training aircraft for the air force as well as for business and work aircraft. The company employs more than 1,300 employees in the Pilatus region of Switzerland and around the globe.
The company’s newest product is the Pilatus PC-21, a training aircraft for a new generation of military pilots. It follows the company’s highly successful PC-12, which is currently the biggest selling single-engine commercial aircraft in the world. There are currently more than 130 on order. This success is no coincidence. It is based on a passion for flying, an obsession for perfection and a willingness to meet customers’ expectations.
The PC-21 not only performs better than the other turboprop aircraft, it is also more economical and quieter. With a top speed of 325 knots/hour for horizontal flying and load limits of -4 G to +8 G it is very suitable for basic and advanced fighter pilot training. Its avionic system is based on an open architecture, with all display systems controlled by software and adaptable to the cockpit environment of each fighter jet. The PC-21, together with instrument and flight simulators, forms an integral part of air force training systems.
Pilatus developed the PC-21 using NX™ digital product development software and Teamcenter® digital lifecycle management software. When Pilatus had to decide between NX and Catia, the company chose NX because its CAM functionality was more powerful. “The decisive question was, ‘Do we want to draw or do we want to produce?’” says John Senior, vice president of Pilatus’ research and development department. “The answer was clear: ‘Produce, with NX.’”
Pilatus carried out the design, development and manufacturing of the PC-21 in parallel, because time to market was critical to the plane’s economic success. “We performed all processes in parallel, and carried out the digital modeling according to the master model concept using only a single model,” says Bruno Cervia, project manager at Pilatus, summarizing one of the most important factors for success. “We never worked on different versions of the model.” Concurrent engineering only works when, as with NX and Teamcenter, design and data management systems are tightly integrated. The NX/Teamcenter combination offered other great benefits as well – saving time and making release changes easier – according to Hännes Keller, technical IT manager at Pilatus.
Keller notes that the cooperation between Pilatus and Siemens was and is very intensive, noting, “We value this collaboration highly.”

Links relacionados:
Cambios:
Claves de Éxito:
Resultados:
Industria:
Actividad Principal del Cliente :
Pilatus Aircraft Ltd is the world market leader in the manufacture of single-engine turboprop aircraft and the only Swiss company to develop, produce and sell aircraft and training systems all over the world.
Sector:
Soluciones/Servicios:
Localización del cliente:
Stans
Switzerland
"The decisive question was, 'Do we want to draw or do we want to produce?' The answer was clear: 'Produce, with NX.'"
John Senior
Vice President, Research and Development
Pilatus Aircraft, Ltd.
Lluís Muntadas, 5 5º planta
Cornellà del Llobregat 08940
Spain
(tlf): +34 93 510 22 00
Share this page through any of the following channels.