In times of increasing cost and time pressures in production, along with ongoing globalization, logistics is a key factor in the success of a company. Money can be lost daily through inefficient schedules, local instead of global optimization, inefficient resource allocation, and poor productivity. The need to deliver just-in-time (JIT) or just-in-sequence (JIS), introduce Kanban, plan and build new production lines, and manage global production networks requires objective decision criteria to help management evaluate and compare alternative approaches.
Plant Simulation is a discrete-event simulation tool that helps you to create digital models of logistic systems (such as production), so that you can explore a system’s characteristics and optimize its performance. These digital models allow you to run experiments and what-if scenarios without disturbing existing production systems or – when used in the planning process – long before the real production systems are installed. Extensive analysis tools, such as bottleneck analysis, statistics and charts let you evaluate different manufacturing scenarios. The results provide you with the information needed to make fast, reliable, smarter decisions in the early stages of production planning.
Using Plant Simulation, you can model and simulate production systems and their processes. In addition, you can optimize material flow, resource utilization and logistics for all levels of plant planning from global production facilities, through local plants, to specific lines.
Capabilities
Benefits
5800 Granite Parkway
Suite 600
Plano, TX
75024
USA
(v): +1 800 498 5351
Share this page through any of the following channels.