Plant Simulation

Product Overview

In times of increasing cost and time pressures in production, along with ongoing globalization, logistics is a key factor in the success of a company. Money can be lost daily through inefficient schedules, local instead of global optimization, inefficient resource allocation, and poor productivity. The need to deliver just-in-time (JIT) or just-in-sequence (JIS), introduce Kanban, plan and build new production lines, and manage global production networks requires objective decision criteria to help management evaluate and compare alternative approaches.

Plant Simulation is a discrete-event simulation tool that helps you to create digital models of logistic systems (such as production), so that you can explore a system’s characteristics and optimize its performance. These digital models allow you to run experiments and what-if scenarios without disturbing existing production systems or – when used in the planning process – long before the real production systems are installed. Extensive analysis tools, such as bottleneck analysis, statistics and charts let you evaluate different manufacturing scenarios. The results provide you with the information needed to make fast, reliable, smarter decisions in the early stages of production planning.

Using Plant Simulation, you can model and simulate production systems and their processes. In addition, you can optimize material flow, resource utilization and logistics for all levels of plant planning from global production facilities, through local plants, to specific lines.

Key Capabilities and Benefits


  • Object-oriented models with hierarchy and inheritance
  • Open architecture with multiple interface support
  • Library and object management
  • Genetics algorithm for optimization
  • Energy consumption simulation and analysis
  • Value stream mapping and simulation
  • Automatic analysis of simulation results
  • HTML-based report builder


  • As much as 6 percent savings upon initial investment
  • Increase existing system productivity by as much as 20 percent
  • Reduce new system costs by as much as 20 percent
  • Optimize resource consumption and re-use
  • Reduce inventories by as much as 60 percent
  • Reduce throughput time by as much as 60 percent
  • Optimize systems for reduced energy consumption
Close share layer

Share this page

Share this page through any of the following channels.

Bookmarking Sites



Blogs & Microblogs