25 May 2010
An integration wrapper between the D-Cubed™ software 2D DCM (Dimensional Constraint Manager) component and Teigha™ for .dwg files is now available from Siemens PLM Software. The wrapper enables users of the Open Design Alliance (ODA) Teigha development platform to introduce the 2D DCM into their products more rapidly.
The 2D DCM solves geometric constraints and driving dimensions to provide the parametric sketching capability in many of the world’s leading CAD systems, including AutoCAD® software from Autodesk, as well as Siemens PLM Software’s own NX™ software and Solid Edge® software. Teigha for .dwg files offers ODA members a development framework for CAD and technical graphics applications that need to support the Autodesk DWG™ file format. Being the same solver as that used in AutoCAD, ODA members that choose to license the 2D DCM can offer their end-users the maximum compatibility with DWG files from that application.
Arnold van der Weide, President of the Open Design Alliance, stated, “The D-Cubed 2D DCM is recognized as the leading geometric constraint and dimension solver. ODA members that choose to license the 2D DCM can deliver constraint solving capabilities combined with DWG file format compatibility to their end-users through their custom applications. Several ODA members are already using 2D DCM in parallel, and I am convinced that direct integrations with applications based on Teigha for .dwg will benefit from the accelerated development that this wrapper delivers.”
If you would like to learn more, please contact us at d-cubed.sales.plm@siemens.com.
Note: Siemens and the Siemens logo are registered trademarks of Siemens AG. D-Cubed, NX and Solid Edge are trademarks or registered trademarks of Siemens Product Lifecycle Management Software Inc. or its subsidiaries in the United States and in other countries. Teigha is a trademark of Open Design Alliance. DWG is the native and proprietary file format for AutoCAD and a trademark of Autodesk, Inc. All other trademarks, registered trademarks or service marks belong to their respective holders.
Decrease Text Size Enlarge Text Size Text Size
Park House, Castle Park
Cambridge, Cambridgeshire
CB3 0DU
United Kingdom
(v): +44 1223 722600
Share this page through any of the following channels.