In this example, the height of a profile is modified interactively. As the distance dimension is increased, the lengths of the vertical edges in the base loop and its offset (top centre) diminish. Eventually these edges pass through zero length and adopt a new direction.
These changes are managed automatically by the PGM, enabling the application to present an intuitive profile modification to the end-user.