Finite element analysis (FEA) is the modeling of products and systems in a virtual environment, for the purpose of finding and solving potential (or existing) structural or performance issues. FEA is the practical application of the finite element method (FEM), which is used by engineers and scientist to mathematically model and numerically solve very complex structural, fluid, and multiphysics problems. FEA software can be utilized in a wide range of industries, but is most commonly used in the aeronautical, biomechanical and automotive industries.
A finite element (FE) model comprises a system of points, called “nodes”, which form the shape of the design. Connected to these nodes are the finite elements themselves which form the finite element mesh and contain the material and structural properties of the model, defining how it will react to certain conditions. The density of the finite element mesh may vary throughout the material, depending on the anticipated change in stress levels of a particular area. Regions that experience high changes in stress usually require a higher mesh density than those that experience little or no stress variation. Points of interest may include fracture points of previously tested material, fillets, corners, complex detail, and high-stress areas.
FE models can be created using one-dimensional (1D beam), two-dimensional (2D shell) or three-dimensional (3D solid) elements. By using beams and shells instead of solid elements, a representative model can be created using fewer nodes without compromising accuracy. Each modeling scheme requires a different range of properties to be defined, such as:
To simulate the effects of real-world working environments in FEA, various load types can be applied to the FE model, including:
Types of analysis include:
Typical results calculated by the solver include:
FEA can be used in new product design, or to refine an existing product, to ensure that the design will be able to perform to specifications prior to manufacturing. With FEA you can:
Here are examples of FEA software applications:
NX Nastran is a finite element solver that analyzes stress, vibration, structural failure/durability, heat transfer, noise/acoustics and flutter/aeroelasticity.
Femap is a CAD-independent, Windows-native pre- and post-processor for advanced engineering FEA. It provides engineers and analysts with an FEA modeling solution to handle even the most complex tasks easily, accurately and affordably.
Solid Edge Simulation is a built-in FEA tool for design engineers to validate part and assembly designs digitally within the Solid Edge environment. Based on proven Femap finite element modeling technology, Solid Edge Simulation significantly reduces the need for physical prototypes, thereby reducing material and testing costs, while saving design time.
The following software components are used by FEA software developers as the foundation for their applications:
Parasolid is 3D geometric modeling component software, enabling users of Parasolid-based products to model complex parts and assemblies. It is used as the geometry engine in hundreds of different CAD, CAM and CAE applications.
Decrease Text Size Enlarge Text Size Text Size
FEA is an integral part of computer-aided engineering (CAE) and a larger product lifecycle management (PLM) strategy. Used together with computer-aided design (CAD), computer-aided manufacturing (CAM), digital manufacturing, and product data management (PDM), entire product lifecycles can be optimized for suitability, reliability and profitability.
5800 Granite Parkway
Suite 600
Plano, TX
75024
USA
(v): +1 800 498 5351
Share this page through any of the following channels.