Faster cycle times made possible by Solid Edge, Femap and Teamcenter improve customer responsiveness
Everdigm produces a wide range of construction machinery as well as equipment for fighting fires and responding to other natural disasters. The company began in 1994 trading second-hand construction machinery. Through constant research and development (R&D) into the production of attachments, concrete pump trucks and tower trucks, Everdigm made the leap into producing its own machinery. Today, Everdigm sells its products locally as well as outside South Korea. Its equipment is exported to more than 60 countries around the world, including the Americas and Europe.
As Everdigm’s business areas were expanding and product variety increasing, management realized the limitations of the company’s 2D design software. It was difficult to create complex shapes with the 2D program, and difficult to reduce defects caused by design errors. In addition, it was getting harder to meet customers’ demands for quicker delivery with the 2D approach. As a result, the company decided to implement a 3D design system.
In choosing the new system, Everdigm was hoping to reduce design time, automate repetitive processes and maintain high-level security of design data. After thorough benchmarking of various 3D computer-aided design (CAD) systems, Everdigm chose Solid Edge® software from Siemens PLM Software. Other factors in favor of Solid Edge were the ease of maintenance, good support, the software’s ability to handle large assemblies and its short learning curve.
Solid Edge provides Everdigm with a robust drafting tool and supports the use of existing 2D data. The use of Solid Edge facilitates the generation of bills of materials (BOMs), exploded views and animations. It also includes a simple macro function for increasing efficiency. Furthermore, the use of Solid Edge will allow the company to expand in the future to product lifecycle management (PLM), another major reason behind Everdigm’s choice.
Along with its deployment of Solid Edge, Everdigm also implemented Femap™ software, a finite element analysis (FEA) pre- and postprocessor from Siemens PLM Software. Everdigm tested the two programs at its ATT R&D center, and then rolled them out to the product development team of each department. The company also provided internal and external training according to the needs of each business area, covering areas such as the use of existing 2D drawings, and 3D modeling and assembly processes. The upgrade to 3D took six months.
Using Solid Edge, Everdigm has increased efficiency by automating repetitive design tasks. For example, Solid Edge permits sequences of material numbers to be transmitted to the enterprise resource planning (ERP) system. It allows drawings to become templates, standardizes file properties and user-entered data, automatically creates the BOM, and permits fast searches of product and BOM data.
With 3D design, Everdigm has been able to decrease the number of defects. The company has also been able to manage product-related data (including design, manufacturing, sales and marketing information) using an integrated database to achieve its main business challenge of working more efficiently.
Since deploying Solid Edge and Femap to create a highly automated 3D design process, Everdigm has achieved outstanding benefits. These include a greater than 15 percent reduction in design time for a first prototype and a 30 to 50 percent reduction for design changes and for the production of a model for mass production. Using Solid Edge has also helped the company determine areas that will be difficult for manufacturing. Having a 3D model and design database connection, the company has achieved 100 percent data consistency between BOM data and drawings, enhancing product and inventory management.
In addition to shrinking the design cycle, Everdigm has been able to enhance design quality and prevent downtime. Solid Edge 3D data is used to create images for use in external marketing, achieving the effect of “killing two birds with one stone.” In the future, Everdigm plans to systemize its overall processes and implement PLM to further increase its efficiency and productivity and significantly reduce time-to-market for its products.
As the level of product complexity increased the amount of CAD data being produced, Everdigm realized that it also needed a more effective data management system. For this, the company started using Teamcenter® software, preconfigured for rapid deployment and fast return on investment, also from Siemens PLM Software. The use of Teamcenter allows Everdigm to integrate and manage all of the data created across its product lifecycle. It also enables more effective collaboration, further reducing design times. Everdigm expects Teamcenter to increase work efficiency by 15 percent.
Related Links:
Challenges:
Keys To Success:
Results:
Industry:
Client's Primary Business:
Everdigm produces construction machinery as well as equipment used in fighting fires and other natural disasters.
Business Initiatives:
Solutions/Services:
Client Location:
Chungcheongbuk-do,, Jincheon-gun, Jincheon-eub
South Korea
"Using Solid Edge, we achieve the effect of having one employee do the work of several people."
Hwang Un Kyoo
Design Engineer, Attachment R&D
Everdigm
5800 Granite Parkway
Suite 600
Plano, TX
75024
USA
(v): +1 800 498 5351
Share this page through any of the following channels.