Jig & Fixture Department
History: The main CAD system for HMC is Catia. However, the Automation Division in charge of jig and automationline design purchased and started using Solid Edge software in 1998. Hyundai’s major challenge was translating Catia data for use in Solid Edge, which resulted in data loss and poor surface handling functionality. In 2002, HMC conducted a benchmark test with Catia and Solid Edge. During the test, Solid Edge received high marks in its operational capability and large assembly handling. As a result, Solid Edge was reselected for continued use. Enhancements to Solid Edge’s surfacing functionality – Rapid Blue and Catia data translation – improved to an acceptable level by using Catia translation software from Radial Soft, a Solid Edge Voyager Program application. The use of Solid Edge is spreading within HMC, which plans to use Solid Edge data to collaborate with its suppliers.
When HMC’s entire jig line is designed, an assembly composed of about 35,000 to 70,000 parts is created. The large assembly handling capability of Solid Edge is absolutely critical to HMC. The library also takes a very important role. Pneumatic cylinder product suppliers in Korea such as FESTO and SMC use Solid Edge to model their product libraries and provide these libraries to HMC.
HMC is considering integrating its systems with its suppliers, some of which are already using, or considering Solid Edge as their main CAD solution for effective collaboration with HMC. HMC’s success with Solid Edge is a very significant factor in influencing other Korean automotive manufacturers and their suppliers to adopt Solid Edge. In addition, HMC plans on using Siemens’ Teamcenter system and its lifecycle visualization capabilities in conjunction with their Solid Edge data to facilitate overall jig line visualization and product simulation.
Currently the Technical Automation Division of Hyundai Motor Company is using 34 seats of Solid Edge. Solid Edge was selected for its high performance operational efficiency and its ability to handle large assemblies for designing automotive jig and production lines.
Advantages of using Solid Edge:
Reseller Youngchang CAD has worked with HMC to develop libraries and an automation program to apply to jig design. This automation program enables designers to extract critical design points from the Catia data that they use when working with Solid Edge on jig design projects. This automation program is crucial to enhancing jig design productivity.
Related Images
Related Links:
Challenges:
Keys To Success:
Results:
Industry:
Client's Primary Business:
HMC is the major automotive manufacturer in Korea, with marques including Hyundai and Kia. HMC employs 50,000 people worldwide and sells cars to 166 countries. The Group also includes over two dozen auto-related subsidiaries and affiliates.
Business Initiatives:
Solutions/Services:
Client Location:
Ulsan City
Korea
5800 Granite Parkway
Suite 600
Plano, TX
75024
USA
(v): +1 800 498 5351
Share this page through any of the following channels.