An industry standard for over 40 years, Nastran is a finite element solver for stress, vibration, structural failure, heat transfer, acoustics and aeroelasticity analyses. Major manufacturers rely on NX Nastran for their critical engineering computing needs, so that they can produce safe, reliable and optimized designs within increasingly shorter design cycle times.
Over 40 enhancements have been made in NX Nastran 8, including the following key areas.
Siemens is making significant investments to expand NX Nastran’s solution capabilities, so analysts can use a common solver to address a broader range of problems. Highlights of discipline and physical domain extensions in NX Nastran 8 include:

Analysis models today can routinely be on the order of 10 to 20 million DOFs in size. As computer hardware continues to improve, analysis model sizes also continue to grow. Siemens makes sure NX Nastran’s solver performance keeps ahead of the pace so that you can efficiently solve ever-larger analysis problems. Computational performance and numerical accuracy improvement highlights available in NX Nastran 8 include:

NX Nastran 8 simplifies modeling, solution set-up and results postprocessing. Highlights of these improvements in NX Nastran 8 include:

3 Knoll Road
Camberley, Surrey
GU15 3SY
UK
(v): +44 1276 702000
Share this page through any of the following channels.