Siemens PLM Software (DK) AS
Birkemose Allé 33, DK-6000 Kolding, Danmark

The following contracts and forms are used for various Academic Processes and can be downloaded from this site.
Current Academic Partners are entitled to free Center-Based Training, to locate the facility closest to the academic institution please review the following classes listed on the Training Web Site. Pick the class of your choice, with 2 alternative and fax form back to the GO PLM office: 314 264 8930.
This form is used to change the network server, i.e. LMHostid and or IP Address on Academic Software accounts. And to cancel the Siemens PLM Software renewal academic licenses. The cancellation will take effect 60 days from the date of this request.
This is the standard contract used for the sale of Siemens PLM Software licenses and standard services issued to our customers and GO PLM Partners.
This contract should be used when licensing a single copy of academic software to a college student or faculty member.
The grant application is used to aid in the processing of in-kind academic software requests. It is reviewed, signed and approved by both the Regional PLM Software Executive and the Director of the GO PLM Program. The information gathered is used for internal tracking purposes and must be issued to ensure prompt and sufficient software ordering processes.
Siemens PLM Software Inc
GO PLM
13690 Riverport Dr.
Attention: Hulas King
MS 285
Maryland Heights, MO 63043
314-264-8930 (fax)
Birkemose Allé 33, DK-6000 Kolding, Danmark
(tlf): +45 70 10 19 48